Hi,
Does CC1125 support the frequency range of 405-410MHz?
Is there any method to spread the frequency range?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For 205 - 240 MHz the data sheet says "Please contact TI for more information about these frequency bands".
I am looking for a part to design a 25 KHz channel FM link with 4KHz deviation in the 216-225 MHz band. Will the CC1125 be ok or is there another more suitable part?
The CC112x family will be fine for this frequency range and setting.
Regards,
Richard
I have the CC1120 development kit with CC1120EM 868/915 MHz (EM). I would like to change the operating frequency band to 216-225MHz. How can I design the RF matching circuit for 216-225MHz operation? Is there any guidline or impedance data for the PA and LNA ports of the CC1120?
The data sheet says it supports 205-240MHz. Is there an application schematic for it?
Hi,
Use the 169 MHz schematic as a base for your design.
http://www.ti.com/tool/CC1120EM-169-RD?keyMatch=cc1120emk-169&tisearch=Search-EN
The balun and LPF can be tweeked slightly but the 169 MHz design is a very good starting point.
Regards, Richard
I have been testing the CC1125 at 230 MHz and altered the BOM for this freq. This BOM will also work for CC120x. I started with testing the 169 MHz BOM http://www.ti.com/tool/cc1125em-169-rd and the CC1120 315 MHz design http://www.ti.com/lit/an/swra398a/swra398a.pdf. Note that if running with the 169 MHz design, you will loose a lot due to the filter. So, the BOM I ended with was this:
For the TX part I used the 433 MHz/315 MHz reference design BOM, the RX part and filter have the following comp values: L191 100n, L192/L201 68n,C201/ C191 10p,L193 33nH, C181 10p, L173 62n, C175 10p, L174 62n. With this BOM for the CC1125 I did not loose sensitivity nor output power, but the 2nd harm might need some more tuning as this was -25 dBm (15 dBm output power). The other harm were below 50 dBm.
I hope this is enough to get you started. Let me know if anything was unclear.
Thank you very much CHS. I will modify my 868/915 MHz EM as per your suggestions and measure the performance before optimising for my narrow operation band of 216-225 MHz.
Thanks Richard. I see the 169MHz operates up to 192MHz - fairly close to the lower end of my band.