Hi
I would like to use the LBT feature of the CC1200. SWRU346B provides some information on the LBT algorithm as defined in EN 300 220. I have a couple of questions I hope someone can answer:
Where is the LBT RX signal threshold set?
Am I correct in thinking that the CC1200 will wait forever if the RX signal level is above the threshold?
Thanks
Bill