Hello,
I am now currently using CC1111F32 USB dongle as the receiver and transmitting the data from the trasnmitter board having same RF circuit as the CC1111F32.The data is being transferred after every 1 second from the transmitter to Receiver (CC1111F32 USB dongle) and is being didpalyed on the monitor.
I am using TI's- simpliciTI with RF frequency of 869.524963 MHz , channel spacing of 199.951172 kHz and modulation technique as GFSK.
It is working fine but can someone explain what will(can) be the difference in using the RF frequency from the other two bands of
433.050 – 434.790 MHz (ETSI EN 300 220)
2400 – 2483.5 MHz (ETSI EN 300 440 or ETSI EN 300 328)
instead of using RF freuency from the 863.0 – 870.0 MHz (ETSI EN 300 220)v band(currently uisng band)
Thanks.