Hello, all
I am working with CC1020 radio transceiver and I observed a characteristic in my receiver: when receiving data, my DLCK is not triggered in a constant frequency. I say that because my transmitter DCLK is triggered at 5k Hz frequency.
Reading the CC1020 datasheet I observed that I should use DCLK as an interrupt input (to my msp). Actually, I'm not using it as an external interrupt because the pin in which the DIO is connected in my microcontroller does not support external interruptions. What I did was setting up a timer to interrupt at 9,5K Hz frequency, sampling the states of DCLK pin and then fetching the data (this worked well for the TX side).
So my doubts are: Why is the DCLK clock in RX mode is not constant as it is in TX mode? A not constant clock in RX mode is a normal operation (and that's the reason why datasheet says I should use external interruption)? Or am I forgetting something when configuring RX mode?
Thank you for your help.
Fávero