Hi,
I am using SimpliciTI 1.2.0 on CCS6 together with MSP430ware 1.80.01.03. Unfortunately there is one inconvenient thing: SimpliciTI defines the stdint types in bsp_msp430_defs.h, whereas MSP430ware is using the definitions of the compiler supplied clib (stdint.h). Usually I don't like to change header files external software, so my wish for the next release would be for SimpliciTI to also include stdint.h - it exists in IAR as well as CCS, so the result would be the same.