Hi,
I think has been described through the authentication is for T67 ARIB STD the CC1120 / CC1200 / CC1175.
Can you tell us about the following points?
1. Do you have a Reference Design you Test the ARIB STD T67 in CC1120 / CC1200 / CC1175?
2. Do you have any Register settings you Test the ARIB STD T67 in CC1120 / CC1200 / CC1175? (Can also set value of SmartRF Studio)
3. In order to pass the ARIB STD T67, crystal oscillator of 32MHz accuracy of ± 4ppm is necessary? Do you have a model number to be recommended if necessary?
Best Regards,
hamada