When register settings for a CC1125 that work in SmartRF Studio ver 7 are exported to use in the Easylink config file "cc112x_easy_link_reg_config.h", does it matter which Template you use? I chose the "trxEB RF Settings Value Line" template (since there was no "Easy Link" template) and pasted those register settings into the "cc112x_easy_link_reg_config.h" file's section "static const registerSetting_t cc1125PreferredSettings[ ] = { }". I programmed the MSP430s with IAR and a MSP-FET430UIF for both the Tx and Rx radios and the Easy Link test does not work; 'Sent Packets' and 'Received Packets' are both zero. I verified nothing was coming out of the Tx radio with a Vector Signal Analyzer. In order to get the Easy Link test to work with register settings exported from SmartRF Studio, does anything else have to be done?
Thanks so much.