This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

External antenna connected detection circuit

Other Parts Discussed in Thread: CC1190, LMV225

Hi,

the maximum allowable input power to the cc112x is 10 dBm. When an antenna is not connected due to an end-user disconnection, I guess the reflected power could possibly destroy the internal PA. This is scenario is probably more valid when an external PA is used.

I know one could use a directional coupler with a log amplifier in order to detect the reflected power level and give a warning that the antenna is disconnected. However, I was wondering if there is a simpler solution that could be employed to detect if an antenna is disconnected? Some antennas do have a resistor with high value connected to ground inside the antenna, this is great for simple detection. But unfortunately not all antennas do have this feature...

Anyone who has any insight to this issue?