Hi, when I was putting my own PCB in operation, the connection between my board and the CC1200-EVA failed, although I was using the same register settings. Therefore, I connected both board to a Spectrum Analyser and found out that the carrier frequency (437.500) of my board is slighly different by +20 kHz. I'm using a 40 MHz TCXO (TG-5021CG).
Do you have an explanation for this frequency shift?