Hello,
in the reference designs for the CC110l (e.g. http://www.ti.com/tool/cc110lem-868-915-rd), the load capacitor connected to the X_OSC_Q2 pin (C101) is always larger than the one on the X_OSC_Q1 pin (C81).
Is there any cause for that or can I just use the same value as long as the resulting load matches the one of the crystal?
Greetings,
Florian