Hi.
I have two boards with cc1110. Minimum baudrate that I get it's 2.4K. If I put in Smart RF a baudrate of 1.2K, after my boards don't communicate.
What will be the problem?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
I have two boards with cc1110. Minimum baudrate that I get it's 2.4K. If I put in Smart RF a baudrate of 1.2K, after my boards don't communicate.
What will be the problem?
Thanks.
Alcidia,
I hope this helps, if not, please post your findings and I will make further suggestions.
Regards,
/TA
I recommend moving them at least 2 meters apart
It didn't work.
The RX bandwidth of the CC1110 is 58kHz, you need to have the two boards tuned to within 20kHz of each other.
Yes, and the boards work with baudrate of 2.4K... 250K, but with a baudrate of 1.2K don't work yet :(
Alcidia,
Strange, are you using the default configuration parameters as found in SmartRF studio?
Regards,
/TA