While choosing parts for a custom CC1200-based radio module we had some questions regarding the bill of material of the reference design (http://www.ti.com/lit/pdf/tidr180 , http://www.ti.com/lit/pdf/tidr181) since some parts are not available or very expensive at our distributor.
Is it possible to replace some of the NP0 or similar classes caps with X7R/X5R with same tolerances or is the temperature-compensation of the NP0 class always required if NP0 is mentioned?
For example C231 is quite expensive at our distributor if you select the stated class (U2J), however, because we accidently ordered the wrong package, we found out that at least basic transmission between two chips on a desk works even without the C231. So now we wonder if a regular X7R/X5R would suffice.
Concerning the inductors, how do you choose the right inductor as there are much more properties like the Q factor, self-resonance that are not specified by the BOM? Are there some guidelines on how to determine the required minimum values?
In the RF circuitry like the balun or matching network, do you have to consider maximum current or voltage or are they always below the current/voltage properties of standard components?
Best regards,
Matthias