Hi!
I'd like to use the CC1101+CC1190 (following the TI ref design) for an 868.3 MHz application (EU) and I'm confused about which crystal (26 or 27MHz) to use in order to conform with EMI requirements.
In the AN094, TI recommends 27MHz with a sensible explanation: The 864MHz spur of the 27MHz crystal is farther from 868.3MHz than the 871MHz spur of the 26MHz crystal. (As far as I understand, the critical value would be 867.5 MHz)
But in the CC1101 datasheet is written: "For compliance with [...] EN 300 220 [...] it is recommended to use a 26 MHz crystal for frequencies below 869 MHz and a 27 MHz crystal for frequencies above 869 MHz."
What is the explanation for the recommendation in the CC1101 datasheet and which is the best choice for CC1101+SAW filter+CC1190 @ 868.3MHz: a 26 or a 27 MHz crystal?
Thank you in advance
Christian Mallas