Hi,
We have made a design based on CC1120 and MSP430 on 868Mhz/915Mhz.
I would like to sale it as a product, which type of certification's do I need?
Is there some tutorial for these issues?
The design is strait forward: just CC1120 and MSP 430 transmitting at 0->10dBm at about 100kbps short packets of about 16 bytes including all headers(sync word, preamble included)
Each packet is transmitted in an interval of 0.5-3 seconds
Thanks,
Yaniv