Hello,
We are going to add the CC1190 as a range extender in our low power wireless product.
One of the requirements of this design is to maintain compatibility to work at two different frequencies: 868 MHz and 915 MHz. We have been looking for reference designs for the CC1190 to work at both and we found the following:
--- For 868MHz: CC1120-CC1190EM 868MHz Reference Design swrr092
--- For 915MHZ: CC1120-CC1190EM 915MHz Reference Design swrr089
Analysing these reference designs we have some questions about them:
1. If we use these designs, we could have a single PCB (swrr092) for both frequencies and two BOM (one BOM for 868MHz and other for 915MHz). Is it correct to use the same layout for the two frequencies?
2. Is the swrr092 4-layer PCB construction compatible for both frequencies? Is it mandatory to use this PCB construction? Could we change any parameter to reduce fabrication cost?
With these features can we have a PCB that supports both frequencies and two BOM’s, one for each frequency, as shown in the following figure:
The design goal of the company is that if it is technologically possible, to have a unique product that works as optimally as possible for both 868MHz and 915MHz.
3. Is it possible to produce a single design to work at both frequencies?
If correct, what would be the best design choice to have a single product (same PCB and BOM)? Would it be feasible to center the bandwidth on the intermediate frequency? What would be the approximate value of losses in this case? Could this option be a problem for ETSI and FCC regulations?
The following figure represent this option:
4. To enable this design option, we should adapt the design to fit that frequency. At schematic level of CC1120-CC1190EM 868MHz Reference Design, do we have enough elements to adapt the network? Do Texas Instruments have a tool to calculate approximate values of the BOM, or should we fit the frequency at experimental level?
Thank you very much in advance,
Noa