Hi,
I'm new to this forum and wonder if there is any SimpliciTI sample codes available for CC1200 to try out with CC1200DK.
Any help or advise will be highly appreciated.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm new to this forum and wonder if there is any SimpliciTI sample codes available for CC1200 to try out with CC1200DK.
Any help or advise will be highly appreciated.
Thanks.
Hi
There is not support for cc1200 in SimpliciTI but there is a beta release version of SimpliciTI for CC1120 here:
http://e2e.ti.com/support/low_power_rf/f/156/p/207308/734398.aspx.
CC1120 and CC1200 are almost identical with respect to digital features so it should be fairly easy to do the port. Use SmartRF Studio to generate settings and note that even if CC1120 and CC1200 have a lot of the same registers there are some bits here and there that are not the same (or placed in different registers for the two parts). Another difference is the crystal frequency on the EM’s (40 vs 32 MHz). This difference will influence the calculations of different delays etc.
BR
Siri