hello, We use a CC1120 that perfectly receive 434Mhz but we have a problem with the values of RSSI . The indications are correct once the offset adjusted but the dynamic is not there . We will as about -80 to -120dBm . Impossible to go over the -80dBm. So dynamic of 40dB instead of 70dB in the worst case. . (values read on RSSI0 and 1 are Ox214 for an AGC_GAIN_ADJUST register of 0 in the case of saturation to -80dBm : So Ox214=532*0.0625=33.25-102(offset)-15(custom adjust for extern LNA) = -83dBm value of saturation for us. )
We use a configuration 4GFSK 163.2kbps Chan_BW = 200kHz . The value of " AGC_REFERENCE " has been adjusted for an external LNA (16dB) . The AGC registers are configured in this way : CFG0 = CB CFG1 = A9 CFG2 = 20 CFG3 = 91
Thanks to explain us what register can be influence the dynamic of measurment of RSSI.
Best regards,
ps : We have try to change the IF_Config that is the value by default or the configuration of DC_Filter but any results on RSSI dynamic