Hi,
I'm designing a board with the CC1200 transceiver and I need to pass the R&TTE and EMC tests.
MY OPINION:
The CC1200 transceiver has a very high level of saturation (10 dBm) but that doesn't prevent from blocking.
10 dBm is very good when no interfering signals are present.
Out-of-band interfering (blocking) signals greater than -40 dBm can still prevent the reception from being correct.
QUESTION 1:
Very high level of saturation doesn't prevent from blocking when interfering signals are present.
Do you agree?
QUESTION 2:
Why do you state in the datasheet that the saw filter is not needed?
Thank you in advance,
Enrico Migliore