I will be using multiple CC1200's in Receive Only mode and Transmit Only mode. One PCB will use four CC1200s in Receive Only mode and one CC1200 in Transmit Only mode; the other PCB will use eight CC1200s in Receive Only mode and two Cc1200s in Transmit Only mode. Obviously, it would be desirable to remove unnecessary components. There is a reason for this configuration - trust me.
Referring to the CC1200EM_866_915 Reference Design Schematic (SWRR121), for Transmit Only operation, I assume that I can remove all six passive components connected to the LNA_P and LNA_N pins (L191, L192, L193, L201, C191, C201) as well as C161. Is that correct? Can the LNA pins be left open, or do they require a DC connection to the TRX_SW pin? For receive only operation, it's not so clear. Can the PA "pull up to VDD" be removed (L171, R171, C173, C171, C172)? Can C174, C176, and L172 also be removed?
I realize that a similar question was asked a few months, but the answer wasn't clear.
Thanks.