Hello ,Im using cc1200 development kit.Im testing the PER For different attenuations.
why the RSSI Increases when i increase RX Filter bandwidth?
Im using a 95Db attenuator between TX and RX,so when i use the 1.2Kbbps,10.96Khz Bandwidth,the packet error is around 81%.But when i increase the RX Filter bandwidth,it came to 0%.And the RSSI Increases correspondingly.
a)1.2Kbps,RX Filter bandwidth=10.96Khz RSSI=>-102.1Dbm.PER=81%
b)1.2Kbps,RX fILter bandwidth=11.90Khz RSSI=>-97.7Dbm.PER=0%
c)1.2Kbps,RX Filter bandwidth=14.88KHZ RSSI=>-89.8Dbm.PER=0%
4)I dont understand why there is reduced packet error when i increase the bandwidth for the same data rate?
Please HELP..Thank you..