Hi,
I have a number of questions here. I'm looking at the CC1120 as a possiblity to use in a product, but I've no expert in RF so hoping to gain some better understanding of the limitations before proceeding with design.
I need up to 30 transmitters, each sending 35byte packets, up to 5 packets per second each to a single receiver. All will be within 300m of each other. I see in the datasheet that CC1120 automates Listen-Before-Send.
1: is there a handshake in the CC1120 packet transmission, so that the transmitter knows when the packet has been received and gets and acknowledgement of some kind? ie - is succesful data transfer thus (eventually) assured?
2: The fixed + random listening time is 5-10ms, so this would limit the possible transmissions to <100 - 200 per second if the transmissions were instantaneous.so thats 3 transmissions from each of my 30 transmitters I guess before things start to get really cramped. I guess in practice there will be collisions and retires with so many transmitters, so throughput would be drastically reduced. This is what makes me think this approach is entirely unsuitable for what I am trying to achieve. can I get a second opinion from someone who knows his onions?
3: If I could manage to convince the customer that one transmission per second was enough, how likely am I to encounter lots of traffic on the same bands from other stuff in the area. Let's assume this product was to be used in a packed olympic stadium.
4: If anyone has any insights into a technology type better suited to my application, I would be very pleased to hear it.
I thank you very much in advance for any input.