Hello,
I'm using the CC1200 set for 500kbps 4-GFSK. All settings except for the actual carrier frequency come directly from SmartRF Studio. I need to get as much data as possible transmitted and received and noticed SmartRF has the default time between packets set to 50ms.
I've been able to reduce that delay in my code while still receiving packets but short of trial and error, is there any way to determine or calculate the minimum time required for the receiver to process the package? It is my understanding that it is the receiver that needs that delay between packets in order to process the packet. I'm currently appending the 2 status bytes but not processing them on the receiver. I am only performing an address check on the receiver then offloading the RX FIFO if packet is accepted.
Can the cc1200 be configured to transmit and receive at a continuous 1Mbps? I looked at the infinite length example but even it introduces a delay between packets. I'm just interested in getting as much data as possible across and any tips to do that would be greatly appreciated.
Thanks,
Juan