Is there a balun that can be used with the CC1310 at 868MHz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mark,
The part number from Johanson will be 0850BM14x0016 were x = variant which is not yet fixed.
The part number from Murata will be LFB18868MBG9E212.
Samples are not yet available.
The balun will cover both 868 MHz and 915 MHz.
Regards,
Richard
Expecting the CC1310 868/915 MHz IPC ref design to be ready in Q1/Q2-2016.
Regards,
Richard
Hi,
The CC13xx IPC 868/915/920 MHz balun should be ready in Q1/Q2-2016.
For the discrete design. Recommend to follow the exact values used in the reference designs since these values have been optimized for both Tx and Rx.
Regards,
Richard
Will the Johanson or Murata part be the same footprint layout as any existing part?
Hi Richard,
Whether integrated Balun for CC1310 is available now.
Regards,
Kamesh
Hi,
The CC1310 IPC can replace all the passives connected to the RF_P, RF_N and RX_TX pads in the standard ref design that covers 779 MHz to 928 MHz.
Johanson part number for CC1310 IPC: 0850BM14E0016
For the Johanson CC1310 IPC datasheet, please contact ijohnson@johansontechnology.com or mcarmona@johansontechnology.com.
Samples will be available in August and RTM in September.
Attached ref design for the evaluation module.
Regards,
Richard
The Johanson balun is going to require a bias voltage on pin 2 which connects to "RX_TX bias" of the 1310 radio. How do I know what voltage is needed on that pin or does the radio generate that. A simpler version of the question is "Do I simply connect RX_TX bias" to the "RX_TX" pin of the balun?
Hi Edouard,
The CC1310 IPC (Integrated Passive Component) from Johanson Technology is finalized. Samples are now available.
See attached reference design for the CC1310 IPC.
Please contact Manuel Carmona <mcarmona@johansontechnology.com> or Ian Johnson <ijohnson@johansontechnology.com> for the IPC datasheet.
There will be an application note (SWRA524) as well to accompany the reference design. This should be on the net during August month.
Copy the reference design. In particular the distance from the IPC to the chip should not be changed.
Regards,
Richard
New 0850BM14E0016 from Johanson for CC1310 is the same size, 1.6x0.8, as the Murata part.
hellow :
for CC1310IPC4XD-7793 Rev 1_0_1 disign files ,We will also use this antenna ;
so would you like to tell me Antenna Match components Value ( C16 L15 L15 R2 )
B.R