Hi
I need help regarding CC1110F32 Real time Clock generation.
Let me explain you little info about this
- I have around 50+ ( FIFTY PLUS) CC1110 Modules ( Perfectly working and genuine )
- Where I'm running custom TCP/IP stack and ISM 868Mhz custom radio communication stack which is communicating with LAN/WAN via router.
- Currently I'm not bothered about power saving modes(none of my devices will never sleep).
- All GPIO's are connected to external devices. ( Please do not suggest me to use external RTC IC's after reading my Qns).
- Using NTP I'm able to synchronize and storing real time in a variable. ( I can re- sync NTP only after 72Hours)
- My engineers are trying with 26Mhz clock with timers which are highly inaccurate reading I'm observing.( failed to get proper timer running)
Now I want to keep a timer running which should be accurate. I have 26Mhz clock and 32.768Khz crystal on board. I will be happy with 1-2 min deviation for every 72hours.
Is it possible to use 32.768Khz crystal to run a timer which can keep my real time running always.( ** My devices will never sleep) independently and i should be able to use other CC1110F32 features ruining at 26Mhz clock.( Radio + SPI+ PWM+ software I2C+ ADC will be always on)
Please can anybody guide me how can i use 32.768Khz Crystal to run a timer accurately ( Please do not tell me to re-syn real time Using NTP which is there in my software)
Please let me know if any info is required from my side. If its not possible I may have to switch to some other SOC. Its urgent Please Guide me how i can handle this.
Regards
Sumanth Kashyap H R