there is a subsidiary carrier wave occur when CC1125 transmit a carrier wave complete,why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Did you test at other frequencies (for example 459MHz & 461MHz)? Does the spur follows the carrier ( same Delta in frequency)? Just I want to make sure that the Spur you are seeing from the board not from external sources.
This spur could be related to the Reference crystal.
What crystal/TCXO freq is being used on the board?
Is this a conductive or radiative measurement?
Thanks,
PM
The upper picture looks like you send a preamble. Are you sure you are actually sending a CW?
Hi,
the situation of subsidiary carrier wave is still after new try which avoid the spurious emissions.there is a spurious emissions occur only when the RF channel is closer than 1 MHz to multiples of XOSC in TX,according to the description of 4.14 in the datasheet.But,when my frequence is set to 422.625MHz,and XOSC is use 40MHz crystal,the spurious emissions occur still.
is there any good advice for me?
thanks.
A spur will not move around randomly, I don't get a spur on the given frequency.
Hi,
if the plot come from SmartRF which show in the e2e_plot2.WMF?Can you show me all registers content of the CC1125 at the moment you send?i mean,if you can read out all the registers and show me the content when CC1125 prepare sending data right away?
thanks,