Hi,
I have couple question related to CC1190.
1. From SmartRF studio, when I select chip CC1101 and enable range extender, EMrev select 915M. I noticed Xtal freq is chenged from 26M to 27M. Does that mean the crystal install on the EM board is 27MHz? Or should I change it back to 26M in config page?
2. PATABLE setting from section 4.2 (www.ti.com/.../swra361a.pdf) , does this setting apply to CC1110 as well?
3. My custom board CC1110+CC1190 is refer to CC1101+CC1190, currently I do not have SAW, if I just shortcut PIN2 and PIN5 with 0 ohm resistor, what could be problem?
4. When I switch CC1190 from receiver state to transmission state, what is the minimum delay that active CC1190 to Tx, and CC1110 can start send strobe STX?
Thanks,
Jason