I apologize if this question seems trivial although I do not have any experience with TI radio and time is short
Currently we use the CC115L TI radio in asynchronous mode and use Timer A to control manchester encoding and timings. I would like to use the normal mode which I assume is writing data in the TXFIFO and letting the chip handle the timings and manchester encoding.
I am wondering what I am missing and need to do in order to switch to this mode. I found the setting in the packet control register and set to normal mode and nothing transmits.
My psudocode would be as followed:
SpiSendCommand( ADD_PATABLE_BURST );
SpiSendCommand( PA_TABLE[0] );
SpiSendCommand( PA_TABLE[1] );
//set test0 register (lost on sleep)
SpiSendCommand(ADD_TEST0_BURST );
SpiSendCommand(rfSettings.test0);
//set TX mode
SendDataToTXFIFO();
//set TX mode
RadioSendCommand(CMD_STX);
Here are my register settings for 345 MHz with my change in PKTCONT0 from asynchronous to normal mode
RF_SETTINGS rfSettings = {
0x00,//0x2E, // IOCFG2 GDO2 Output Pin Configuration
0x00,//0x2E, // IOCFG1 GDO1 Output Pin Configuration
0x00,//0x2E, // IOCFG0 GDO0 Output Pin Configuration
0x47, // FIFOTHR RX FIFO and TX FIFO Thresholds
0xD3, // SYNC1 Sync Word, High Byte
0x91, // SYNC0 Sync Word, Low Byte
0xFF, // PKTLEN Packet Length
0x04, // PKTCTRL1 Packet Automation Control
0x02, //0x32, // PKTCTRL0 Packet Automation Control
0x00, // ADDR Device Address
0x00, // CHANNR Channel Number
0x06, // FSCTRL1 Frequency Synthesizer Control
0x00, // FSCTRL0 Frequency Synthesizer Control
0x0D, // FREQ2 Frequency Control Word, High Byte
0x44, // FREQ1 Frequency Control Word, Middle Byte
0xEC, // FREQ0 Frequency Control Word, Low Byte
0xF7, // MDMCFG4 Modem Configuration
0x20, // MDMCFG3 Modem Configuration
0x38, // MDMCFG2 Modem Configuration
0x22, // MDMCFG1 Modem Configuration
0xF8, // MDMCFG0 Modem Configuration
0x15, // DEVIATN Modem Deviation Setting
0x07, // MCSM2 Main Radio Control State Machine Configuration
0x30, // MCSM1 Main Radio Control State Machine Configuration
0x18, // MCSM0 Main Radio Control State Machine Configuration
0x16, // FOCCFG Frequency Offset Compensation Configuration
0x6C, // BSCFG Bit Synchronization Configuration
0x03, // AGCCTRL2 AGC Control
0x40, // AGCCTRL1 AGC Control
0x91, // AGCCTRL0 AGC Control
0x87, // WOREVT1 High Byte Event0 Timeout
0x6B, // WOREVT0 Low Byte Event0 Timeout
0xFB, // WORCTRL Wake On Radio Control
0x56, // FREND1 Front End RX Configuration
0x11, // FREND0 Front End TX Configuration
0xE9, // FSCAL3 Frequency Synthesizer Calibration
0x2A, // FSCAL2 Frequency Synthesizer Calibration
0x00, // FSCAL1 Frequency Synthesizer Calibration
0x1F, // FSCAL0 Frequency Synthesizer Calibration
0x41, // RCCTRL1 RC Oscillator Configuration
0x00, // RCCTRL0 RC Oscillator Configuration
0x59, // FSTEST Frequency Synthesizer Calibration Control
0x7F, // PTEST Production Test
0x3F, // AGCTEST AGC Test
0x81, // TEST2 Various Test Settings
0x35, // TEST1 Various Test Settings
0x09, // TEST0 Various Test Settings
};
Thanks,
David