In table 5.6 "Receive(Rx) Parameters" of CC1310's datasheet, the row 5 shows that the Rx sensitivity is -110 dBm at 50 kpbs, 1% BER, 868/915MHz and other conditions.
As part of the evaluation, we would like to know the Rx sensitivity values at 0.1% BER and 1% PER, leaving all other conditions the same as those specified in datasheet. So that we can tell if CC1310 can fit the distance requirement in the scenario we're working on.
As we cannot acquire any eval kit yet (sample request is back-ordered while chips for purchases is out of stack), it will be appreciated if some TI staff familiar with the chip can post some more data to address the above questions.