Hi,
I am looking for the OOK receiver for our existing OOK transmitter but I don't sure it is good for using CC1121 or CC1101 for such application. Is there any sensitivity or range enhancement for using CC112x compared with CC1101.
In addition, I cannot find sensitivity reading for the CC112x with OOK operation with 25kHz or 100kHz Rx BW in the data sheet. Can you provide us some reference no. on it.
Finally, I used the smartRF studio with the CC112x kit with transparent serial mode setting and found RSSI value will up to -80dBm if Rx BW is set to 100kHz. Do you think the signal lower than -80dBm will not be receive with such setting?
Thanks,
HungLI