Hi,
We are working on a test setup based on a combination of an MSP430FR5739 Launchpad (which comes with EM slots) + PCBs we got manufactured from the Gerber provided for CC112x (CC112x 2 layer design with IPC - http://www.ti.com/tool/cc112x-ipc-2l-868rd). The parts used are the same and the Balun is the one from Johnson.
We were able to port the Easylink example to the same board, and run with default values. On the transmitter side, we see that the interrupt on successful transmission is raised. But, the receiver side never receives anything!
We have experimented with the on-board PCB antenna but found out that the PCB thickness is wrong (should have been 0.8mm, but it was manufactured using 1.6mm). Now, we have moved to SMA connector + whip antenna. But, results are the same! We have never been able to get anything on the Rx side.
Although we have tried multiple settings in the SmartRF Studio, the current one that we are trying is:
Carrier Freq.: 868.00 MHz
Xtal Freq.: 32.00 MHz
Symbol Rate : 50 ksps
RX filter BW: 100.00 kHz
Modulation format: 2-FSK
Deviation 24.963379 kHz
TX power: 15dBm
Manchester Enable: NO
PA ramping: YES
Whitening: NO
Performance Mode: High Performance
Any guidance on how to go about this would be great!