i have a pair of CC1310 EMs, which are talking to one another under control of smartrf studio.... i'm communicating at 50kbps, using the settings available through smartrf studio....
(at present, i have a CC1101-based system that is communicating at 250kbps (using settings generated under smartrf studio) -- and i need to have my CC1310 interoperate with the CC1101....)
i find, however, that when i increase the datarate (even slightly!!!) on the CC1310 that no communication takes place.... for instance, if i raise the symbol rate to 60 kBaud i don't receive any packets!!!! but, if i *lower* the symbol rate to 40 kBaud, everything continues to work....
(this all started with a set of RF parameters in which the symbol rate was 250K, the deviation was 132K, and the RX filter was 530kH -- parameters that (should) match what i'm using on the CC1101.... this didn't work either....)
at this point, i'm curious if anyone has had a similar experience with the CC1310???? and if you have successfully communicated between CC1310s using smartrf studio, what specific RF parameters did you use????
thanks, bob.