Hello,
I'm testing two CC1200 modules (TI eval modules). I've connected them to st nucleo boards. There's no problem with SPI communication. I'm using the Smart RF Studio Easy mode register settings. I just want to test simple recieve and transmit function between 2 boards.
First problem is that i can't switch any module to RX mode. Stobe RX doesn't work.
Second, when i try to transmit data in TX mode, ı can see that TX FIFO increases but just can't send the bytes and FIFO OVERFLOW occurs.
Can you please summarize the simple prosedure to test basic communication?