I can't make Z-Tool 2.0 work under the windows 7;
It works OK under XP.
From posts on Forums I got impression that window7 and Z-Tool 2.0 are not compatible
Can somebody confirm this for sure?
Thanks,
Nick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If you unable to open the software. right click the and "Run as administrator"
If you are able to open the software . Then Check Tools--->Settings---->Serial Devices ------> Double Click the Com Port (The com port connected to the RS232 Cable)--->Select the option for the handshake to RTS/CTS.
Hope it helps.
Thanks and Regards
Lakshman.
Thanks Lakshman,
I am using Windows 7, 32 bits
1) One W7 machine sports a banner "Please wait " and it never goes away. So I can't even check the settings
Settings for a port are done before starting Z-Tool and I am not sure if they remain that way
2) The other W7 machine reports "no devices found". The settings are correct ( 38K/RTS/CTS) for the second machine
3) No problem with XP machine.
Not a show stopper, I was just curios if somebody runs Z-Tool 2.0 on Windows 7 ( 32 bit ? )
Cheers,
Nick
Hi Friend ,
Where can i get the Z tool 2.0 download or send the link to download.
Hi sivasankar,
You can install Z-Stack Home 1.2.0 and ZTool is at C:\Texas Instruments\Z-Stack Home 1.2.0\Tools\Z-Tool
Hi Friend,
I want try the ZNP(Packet sniffer)<---->ZAP(PC),So i want to program my Packet Sniffer as ZNP so i saw the folder ZNP-HexFiles in my Z Stack HM 1.0 project but in that folder so many ZNP hex files,So i decided to build the ZNP-TestHex (Regaurding from doc).
My Q:
1.From that files which one is best or TestHex files is set for my simple task?
Hi Friends,
I am also using Windows 7,32 bits
I download the z stack home automation for Z tool 2.0 but when i open the software a small window searching something infinitely so i can't use the Z tool .I think my system in win 7 32 bit because of the reason only i can't work and when i search Z tool it simply give the same software.So give any idea to Z tool in Win 7 32 bit.
HI sivasankar,
1. Would you attach the screen snapshot?
2. If you have another PC, I suggest you to test Z tool on it again.
Hi YiKai Chen,
I tried my friend systems also and as i say before only 64 bit systems only working properly in Z tool.
Hi YiKai Chen,
I programed my packet sniffer as ZNP and i install Z tool 2.0 in my PC.When i plugin my Packet sniffer in my PC the Z tool 2.0 detect my device.
My Q:
1.How to conform my PC successfully interface with ZNP device(Packet Sniffer) ?
Every ZNP command has ACK. You can send any ZNP command such as
SYS_VERSION and see if you can receive ACK.
Hi YiKai Chen,
I programed my packet sniffer as ZNP and i install Z tool 2.0 in my PC.When i plugin my Packet sniffer in my PC the Z tool 2.0 detect my device.
My Q:
1.I don't know how to set configid,could you replay me how to know configid or how to set this value?
Hi sivasankar,
Your question is not really related to this thread topic. I would suggest you init a new post and specify the following items:
1. What Z-Stack version do you use?
2. What HW do you use? CC2530zdk or CC2531 usb dongle?
3. What FW do you download to your HW?