Hi,
when trying to send some data using the AF_DATA_REQUEST 0x2401, I get following AF_DATA_CONFIRM:
msg received, command: 0x4480, msg len: 3
recv buff: 1a 02 12
The 0x1A in the recv buffer is status. It is obviously not an OK status. However, I cannot find it's true meaning. On my sniffer I can see no message is transmitted from CC2530 to zigbee network. After several attempts with the same result, I get another bad status message as response for ZDO_NWK_ADDR_REQ 0x2500:
msg received, command: 0x6500, msg len: 1
recv buff: 10
Where 0x10 means - ZMemError
Any ideas?