I am following along on this TI wiki: http://processors.wiki.ti.com/index.php/Contiki-6LOWPAN and I found the source firmware for the cc2538 on Thingsquare's site:
http://www.thingsquare.com/download/thingsquare-mist-1.1.0.zip.
Inside the source there is a file cc2538-demo.c in the examples/cc2538dk folder. I copied the source into the Develop pane of the thingsquare demo site as documented on the wiki and there are no highlighted errors. But when I select a TI device and try to Run the program on that device, I get an error:
Failed to compile the application for the target device.
I see no other messages or explanations. Most of the simple demos I have tried including the Hello World and Blink examples work just fine, copied from the same source folder. But this more extensive one does not.
Can anyone explain what I am doing wrong and perhaps offer a suggestion?