Hi,
The developed software seems ok if cc2538 works with IEEE 802.15.4 stack.
However, when we migrate the software from IEEE 802.15.4 to ZigBee, unexpected problem occurs. If the function of :
ZDApp_event_loop ()
is enabled, the interrupt line, which is pc7, will generate countless interrupt to cc2538, and the system stops working.
My question is, does PC7 on cc2538 have certain internal relationship with ZigBee stack, and the relationship forbids the use of PC7 as interrupt line when ZigBee stack works?
The development tool I am using is IAR 7.20.1.7307
The Zigbee stack is included Z-Stack Home 1.2.0
Debug tool XDS100V3
When problem occurs, the debug interface stops at
void FaultISR(void)
which is defined in startup_ewarm.c
Any suggestion is very much appreciated!