I am trying to go through the Thingsquare 6LoWPAN MSP430 setup from the TI Wiki: http://processors.wiki.ti.com/index.php/Thingsquare_6LoWPAN_MSP430
The description is very clear and everything works up to the section called Running Online Test Client.
WebPage Test Client
- Use Browser and browse to http://mqtt-io-old.herokuapp.com/.
- Input Broker TCP/IP address: 85.119.83.194, port: 1883 and client identifier: Any value
- Subscribe to 3 topics for each node as below.
Topic: ti/iot/device/xxxxx, using QoS 0 Topic: ti/iot/device/xxxxx/state, using QoS 0 Topic: ti/iot/device/xxxxx/led, using QoS 0
I enter the Broker TCP/IP address, port and client identifier and push "Connect" but it stays disconnected. I cannot go any further with the setup. Please help.
JH