Hello,
I use TIMAC 1.5.0 with the CC2531 and I tried power modes PM2 and PM3 to save energy for battery operation. Two questions:
1) In PM3, the MCU core is without clock and according to the user guide, it can wakeup only via an IO event such as an interrupt on P0 or P1. This works for me. But is it correct that I can not wakeup using a timer in PM3 as they are also without clock?
2) I understand that for PM2, the MCU runs with 32 kHz. In my case, the device has a changing current of 25, 80, 180 and 212uA in PM2. Why is that? Do I have to deactivate tasks manually?
To activate PM2, I run:
MAC_MlmeSetReq(MAC_RX_ON_WHEN_IDLE, &_false);
osalApi_PowerMgr(TRUE);
Any advice?