HI,
The application is for Battery monitoring, using ZigBee IEEE 802.15.4 standard, for wireless sensing.
The customer claims that TI app note should advise that this part could be connected as a network more than 400 devices.
However, now the customer can only connect up to 40 devices.
The initial plan is actually to connect at least 430 devices.
Do you have any experience for such application and device? Some kind of case study
Also, the customer is asking for any training or at least some material or tutorial for the application.
Please help or advise.