hi,
i am working with TIMAC and i want to send ADC data.
can someone tell me the spi flow through which the ADC data is being passed through the SPI to the transmission buffer in the CC2520.
i have searched the mac_spi.c file also.
it has two functions which tells about
1)Write value to radio register.(void macSpiWriteRamUint16(uint16 ramAddr, uint16 data))
2)Write unsigned 16-bit value to radio RAM(
void macSpiWriteReg(uint8 regAddr, uint8 regValue))
i am not clear in which register the values from the SPI gets stored in the CC2520 for transmission.
)