How can I get the network addresses/IEEE addresses of all currently active nodes(including the ones outside radio range, e.g., an end device whose parent is inside radio range) ?
Let, I have-
ZC -->ZR1-->ZR2 --> ZED
The ZR1 is inside the radio range of ZC, ZR2 is in range of ZR1, ZED is in range of ZR2. If I store the network addresses by collecting them from device announcements, that gives me the list of all active+inactive(if the ZED is powered off) nodes. How can I get the list of just the active nodes?