Hi
I working on cc2538 and smartRF06EB boards....
My project is to send the sensors data (accelerometer, temperature, PIR, heartbeat) in a packet and should communicate between two smartRF06EB boards...
I would like to put one as a coordinator and other as router...and the sensors data should transmit between two boards.....
My query here is
1.should i use zstack or per test...for my application...
2.which functions are used for packet transmit or receive...