My coordinator is receiving a message type of 0x45B8 from the module. The full message is listed below
1C 45 B8 E8 C5 00 00 F8 FF 07 15 00 08 00 10 88 3F 3C 8D 73 56 5E 71 73 56 4C 6E 73 5E 51 00
What is this message type?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My coordinator is receiving a message type of 0x45B8 from the module. The full message is listed below
1C 45 B8 E8 C5 00 00 F8 FF 07 15 00 08 00 10 88 3F 3C 8D 73 56 5E 71 73 56 4C 6E 73 5E 51 00
What is this message type?
Hello Jill, Which Z-Stack version are you using?
We are using the Anaren A2530E24AZ1GM module. So I am not sure which Z-Stack Version it contains.
Hello Suyash,
I was told the version that we are running is 2.5.1.
No. When a message comes in I look for AF_INCOMING, AF_INCOMING_MSG_EXT, ZDO_IEEE_ADDR_RSP, AF_DATA_CONFIRM, ZDO_NWK_ADDR_RSP, ZDO_END_DEVICE_ANNCE_IND, and ZB_FIND_DEVICE_CONFIRM. Since it is not any of these I print out the raw message.
Hi Jill,
I check ZNP source code and the only response related to this one is "/* 0xB8 */ ((uint8)Mgmt_NWK_Update_req | 0x80)". I suspect this is some NWK work update rsp but there is no document for this. I suggest you try to contact Anaren since this module is made by them.