Hi everyone,
There is a ZED which need to achieve the following functions :
1. when it is detected by the something, it will sending MSG to CIE,and i simulate like a key interruption
2. it was powered by battery , it will checking the battery everyday one time,it will sending the low power MSG,if battery is low
and i want to make this ZED into sleep Mode in when idle。
is that right setting as below:
1. add POWER_SAVING in compilers
2. define RFD_RCVC_ALWAYS_ON=FALSE in f8wConfig.cfg file
3. change some define in f8wConfig.cfg file
-DPOLL_RATE=0
-DQUEUED_POLL_RATE=0
-DRESPONSE_POLL_RATE=0