(Z-stack Home 1.2.1 CC2530)
Hi,
Question 1) If an End Device is issued a new short address, does it get a completely new entry in the Association Table?
Question 2) If the answer to Question 1 is yes, then how to a force a Child (ZED or ZR) to generate/be issued, a new short address?
I am trying to force a new entry in the Coordinator Association Table when an End Device re-parents to a Router. I know Child Aging does this but I need to make it happen as soon as a device re-parents, and not wait for KEEPALIVE timeout value of Child Aging. Setting Child Aging to 0 causes way too many Leave Requests.
Also, I don't use the Short Address in my application, I use the IEEE instead, so it can change with no impact.
(Alternatively, is it possible for the Child Aging timeout value to be dynamically changed? I have tried this but to no avail)
Thanks,
Andy