Hello there !
I'm trying to make use of the CC2650EM on a SmartRF06EB to tame 6LoWPaN with the help of Contiki OS. I'm able to compile and load on the EM the cc26xx-demo furnished within Contiki, using the Flash Programmer v2 software on Windows (although I develop with Ubuntu...).
My problem is the following : I'm using this software to "monitor" the USB-serial port (I'm connected via USB to the EB). While the image seems to be working quite fine (the LEDs and buttons respond as expected), I observe nothing on the serial port. The board is correctly mounted and recognized by Windows 7, and the TI XDS100v3 Channel B is rightly linked to one of my COM port. However, I'm unable to see anything on the corresponding serial port...
What could I have done / am I doing wrong ?
Great thanks in advance for the help !
Cyril