The datasheet talks about a 850mA peak power every 5 minutes.
This is more than 600mA above normal operation of the chip.
I see no mention of which rail gets this peak power (1.8V or 3.3V)
I also see no mention anywhere about how much time this peak last.
This is critical to calculate the power supply.
I am now very close to the PMIC limits of 2A at 5V when I add up all maximum power consumption of every circuits.
Also, is there a software control and/or notification available when this happens so I can shutdown something else?