after creating all the required latest modules for wl18xx module to run on android imx6 custom board based on wandboard, kernel 3.0.35+
I cannot get pass ' ADDRCONF(NETDEV_UP): wlan0: link is not ready'
Here what I get:
[ 5.013089] compat-drivers backport release: ol_r8.a7.02
[ 5.018531] Backport based on wl18xx.git ol_r8.a7.02
[ 5.023663] compat.git: wl18xx.git
[ 5.063093] cfg80211: Calling CRDA to update world regulatory domain
[ 6.054881] wl1271_sdio mmc1:0001:2: sdio PM caps = 0x3
[ 6.401574] wlcore: wl18xx driver version: ol_r8.a8.10
[ 6.405692] add wake up source irq 103
[ 6.436470] yuli - arch/arm/mach-mx6/board-wand.c:wl12xx_set_power: set power(1)
[ 7.087785] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[ 7.192872] yuli - arch/arm/mach-mx6/board-wand.c:wl12xx_set_power: set power(0)
[ 7.282838] wlcore: loaded
[ 7.285729] wlcore: driver version: ol_r8.a8.10
[ 7.290391] wlcore: compilation time: Tue Aug 26 07:03:10 2014
[ 15.009931] warning: `zygote' uses 32-bit capabilities (legacy support in use)
[ 15.030139] alarm_set_rtc: no RTC, time will be lost on reboot
[ 21.394893] request_suspend_state: wakeup (3->0) at 21148467006 (1970-01-02 00:00:06.364766334 UTC)
[ 21.404377] cpufreq_interactive_input_connect: connect to bcd_ap386x
[ 22.068753] yuli - arch/arm/mach-mx6/board-wand.c:wl12xx_set_power: set power(1)
[ 22.196309] acc_open
[ 22.198613] acc_release
[ 24.249044] wlcore: PHY firmware version: Rev 8.2.0.0.195
[ 24.954570] Yuli - wlcore_irq
[ 25.310961] wlcore: firmware booted (Rev 8.8.0.0.13)
[ 26.060364] ADDRCONF(NETDEV_UP): wlan0: link is not ready
[ 26.166480] wlcore: down
[ 26.179009] Yuli - wlcore_irq
[ 26.214882] yuli - arch/arm/mach-mx6/board-wand.c:wl12xx_set_power: set power(0)
[ 26.336468] yuli - arch/arm/mach-mx6/board-wand.c:wl12xx_set_power: set power(1)
[ 28.145659] wlcore: PHY firmware version: Rev 8.2.0.0.195
[ 28.853138] Yuli - wlcore_irq
[ 29.209273] wlcore: firmware booted (Rev 8.8.0.0.13)
[ 30.263452] ADDRCONF(NETDEV_UP): wlan0: link is not ready
[ 30.387052] Yuli - wlcore_irq
[ 30.476467] wlcore: down
[ 30.488924] Yuli - wlcore_irq
[ 30.524746] yuli - arch/arm/mach-mx6/board-wand.c:wl12xx_set_power: set power(0)
[ 30.711195] ehci_fsl_bus_resume begins, Host 1
[ 30.736485] ehci_fsl_bus_resume ends, Host 1
[ 30.758588] ehci_fsl_bus_resume begins, DR
[ 32.914392] init: sys_prop: permission denied uid:1003 name:service.bootanim.exit
[ 33.266536] ehci_fsl_bus_suspend begins, Host 1
[ 33.272034] ehci_fsl_bus_suspend ends, Host 1
root@wandboard:/ #
root@wandboard:/ #
root@wandboard:/ #
root@wandboard:/ # ifconfig wlan0 down
255|root@wandboard:/ # ifconfig wlan0 10.10.10.10
[ 280.656514] yuli - arch/arm/mach-mx6/board-wand.c:wl12xx_set_power: set power(1)
[ 282.600248] wlcore: PHY firmware version: Rev 8.2.0.0.195
[ 283.296070] Yuli - wlcore_irq
[ 283.650938] wlcore: firmware booted (Rev 8.8.0.0.13)
[ 284.616403] ADDRCONF(NETDEV_UP): wlan0: link is not ready
root@wandboard:/ # ifconfig wlan0
wlan0: ip 10.10.10.10 mask 255.0.0.0 flags [up broadcast multicast]
root@wandboard:/ # ifconfig wlan0 down
[ 299.747585] Yuli - wlcore_irq
[ 299.816467] wlcore: down
[ 299.828967] Yuli - wlcore_irq
[ 299.864768] yuli - arch/arm/mach-mx6/board-wand.c:wl12xx_set_power: set power(0)
root@wandboard:/ # ifconfig wlan0 down
[ 304.086486] EXT4-fs (mmcblk0p4): error count: 2
[ 304.091227] EXT4-fs (mmcblk0p4): initial error at 1407311255: ext4_journal_check_start:56
[ 304.099986] EXT4-fs (mmcblk0p4): last error at 1407311255: ext4_journal_check_start:56
root@wandboard:/ # ifconfig wlan0 up
[ 311.156517] yuli - arch/arm/mach-mx6/board-wand.c:wl12xx_set_power: set power(1)
[ 313.100173] wlcore: PHY firmware version: Rev 8.2.0.0.195
[ 313.799758] Yuli - wlcore_irq
[ 314.154675] wlcore: firmware booted (Rev 8.8.0.0.13)
[ 315.049844] ADDRCONF(NETDEV_UP): wlan0: link is not ready
Any help would be appreciated.
Thanks!