Hi, my previous problem not solved, but i can test my board with smartphone.
place my board close to AP. (about 5 cm).
i am testing some network middleware with smartphone app.
sometimes, i think my board seems to be throttle
when it happen, ran "top" command minicom serial terminal,
it happening randomly.
here is the result:
22% [irq/194-wl18xx]
PID PPID USER STAT VSZ %VSZ %CPU COMMAND
1406 1403 root R 58076 23% 45% /home/root/network_server
1118 2 root SW 0 0% 22% [irq/194-wl18xx]
1440 1410 root R 2124 1% 18% top
42 2 root SW 0 0% 3% [kworker/0:1]
1439 2 root RW 0 0% 2% [kworker/u2:1]
1422 2 root SW 0 0% 2% [kworker/u2:2]
1267 1 root S 3000 1% 1% /usr/bin/ntpd -p /var/run/ntp.pid -g
3 2 root SW 0 0% 1% [ksoftirqd/0]
1 0 root S 1324 1% 0% init [5]
1347 1 root S 4832 2% 0% wpa_supplicant -d -Dnl80211 -c/etc/
1389 1 root S 4240 2% 0% hostapd -B /etc/hostapd.conf -P /var/r
819 1 root S 2712 1% 0% /lib/udev/udevd -d
and there is some kernel message about wl1801
here :
root@am335x-evm:~# [ 1066.674409] wlcore: ERROR Tx stuck (in FW) for 5000 ms. Starting recovery
[ 1066.681882] ------------[ cut here ]------------
[ 1066.687201] WARNING: CPU: 0 PID: 1422 at drivers/net/wireless/ti/wlcore/main.c:802 wl12xx_queue_reco)
[ 1066.699897] Modules linked in: ipt_MASQUERADE iptable_nat nf_conntrack_ipv4 nf_defrag_ipv4 nf_nat_ipx
[ 1066.752088] CPU: 0 PID: 1422 Comm: kworker/u2:2 Not tainted 3.12.10-ti2013.12.01 #1
[ 1066.760508] Workqueue: phy0 wl12xx_tx_watchdog_work [wlcore]
[ 1066.766779] Backtrace:
[ 1066.769671] [<c0017880>] (dump_backtrace+0x0/0x10c) from [<c0017a1c>] (show_stack+0x18/0x1c)
[ 1066.778874] r6:bf2189fc r5:00000009 r4:00000000 r3:c07f537c
[ 1066.785465] [<c0017a04>] (show_stack+0x0/0x1c) from [<c0569cd4>] (dump_stack+0x20/0x28)
[ 1066.794210] [<c0569cb4>] (dump_stack+0x0/0x28) from [<c0046d08>] (warn_slowpath_common+0x70/0x90)
[ 1066.803879] [<c0046c98>] (warn_slowpath_common+0x0/0x90) from [<c0046d4c>] (warn_slowpath_null+0x24/)
[ 1066.814266] r8:00000000 r7:cd076400 r6:cc088c20 r5:cc088c54 r4:cc088c20
[ 1066.822274] [<c0046d28>] (warn_slowpath_null+0x0/0x2c) from [<bf2189fc>] (wl12xx_queue_recovery_work)
[ 1066.834109] [<bf218988>] (wl12xx_queue_recovery_work+0x0/0x80 [wlcore]) from [<bf218db8>] (wl12xx_tx)
[ 1066.847342] r4:cc0898d4 r3:00000001
[ 1066.851454] [<bf218cb4>] (wl12xx_tx_watchdog_work+0x0/0x138 [wlcore]) from [<c0059f50>] (process_one)
[ 1066.862943] r6:cd06e800 r5:cc0898d4 r4:cd294d40 r3:bf218cb4
[ 1066.869526] [<c0059e54>] (process_one_work+0x0/0x340) from [<c005a558>] (worker_thread+0x130/0x370)
[ 1066.879376] [<c005a428>] (worker_thread+0x0/0x370) from [<c005fbdc>] (kthread+0xac/0xb8)
[ 1066.888227] [<c005fb30>] (kthread+0x0/0xb8) from [<c00146f8>] (ret_from_fork+0x14/0x3c)
[ 1066.896968] r7:00000000 r6:00000000 r5:c005fb30 r4:cd0b5e74
[ 1066.903525] ---[ end trace 522e3074244c5176 ]---
[ 1066.909534] wlcore: Hardware recovery in progress. FW ver: Rev 8.8.0.0.13
[ 1066.917551] wlcore: pc: 0x0, hint_sts: 0x00000048 count: 1
[ 1066.928000] wlcore: down
[ 1066.931002] wlcore: down
[ 1066.935453] ieee80211 phy0: Hardware restart was requested
[ 1070.879596] wlcore: PHY firmware version: Rev 8.2.0.0.195
[ 1071.058628] wlcore: firmware booted (Rev 8.8.0.0.13)
[ 1071.107231] wlcore: Association completed.