Dear Sirs:
I have ever ask for the WL18xx can fit ETSI 300 893 v1.7.1 or not in the following link:
http://e2e.ti.com/support/wireless_connectivity/f/307/t/368235.aspx
And our customer went to do the pre-test of it at lab, and unfortunatelly, it fails.
It fails on the Adaptivity test, and I also found some same problem is also on 1283 in the following post:
http://e2e.ti.com/support/wireless_connectivity/f/307/p/371337/1307721.aspx#1307721
According to the answer of the post, the fix must be done in TI F/W and not in user side.
So, I would like to know whether the WL18xx firmware has such a fix or not? Or any options that we can set in the driver?
The driver version we are using is WL18xx R8.4
The sdk we are using is 6.0.
Regards,
/ckhsu